2015-10-22 09:20 AM
Hi,
I'm trying to get to grips with System Workbench for STM32 & STM32F429i-Disco board.I'm trying to build the STemWin_SampleDemo project for STM32F429I-Discovery, supplied in STM32Cube_FW_F4_V1.8.0but it comes up with a linker error :w_sqrt.c:(.text.sqrt+0xa8): undefined reference to `__errno'collect2.exe: error: ld returned 1 exit statusI've tried everything I can find suggested here & elsewhere ( mainly revolving around linking the math library with -lm, but this makes no difference.)I was kinda hoping that a project supplied by ST from their STMcube suite using the ST (supplied?) IDE would compile without issue so i could use it as a platform to work from.Other projects, including the 'STM32F429I-Discovery' demonstration project, (also using the STemWin library) build & link without issue.Linker Script: -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -L..\..\..\..\..\..\..\..\Middlewares\ST\STemWin\Lib -specs=nosys.specs -specs=nano.specs -T''..\STM32F429NIHx_FLASH.ld'' -Wl,-Map=output.map -Wl,--gc-sections -lmAny ideas on how to resolve this would be welcomeTIA... DaemyP.S. same project compiles without issue on a Keil/Arm compiler [but I don't have easy access to that :-( ]2015-10-22 10:46 AM
Not sure about your environment, but on a Linux system, _errno is usually located in libc.a, the C library linked in by default, or explicitly invoked by ''-lc''. And by definition, sqrt() sets the errno variable.
You might need to check if you are linking against a proper libc. Alternatively, you might check if your compiler supports the -fno-math-errno option.2015-10-23 03:17 AM
Thanks,..
Environment:Win7(32bit)SP1System Workbench for STM32 (Eclipse-Ac6 STM MCU GCC)MCU: STM32F429errno.h is in the include pathas far as I can tell everything else is as it should be, but I'm kinda new to Eclipse & this MCU (moving up from years spent writing in C for 8051s on Keil C51 compiler) & atm not finding it as easy as I hoped :-(2015-10-23 04:21 AM
errno.h is in the include path
The errno.h header only declares this variable - if you check, usually as ''external int errno;''. You need to link against a library that actually contains this variable. I don't know the System Workbench environment, so I'm not sure how it invokes the standard C libraries. I would start with checking the build log. Does the linker call contain a ''-nostdlib'' option ? Most toolchain keep several versions of the libraries (M0, M3, M4, soft, softfp, hard, etc.) in different paths. Perhaps there is something not setup correctly in your toolchain, or in your project settings ? Is there no ''System Workbench'' help regarding library usage ?
2015-10-23 06:08 AM
Thanks for your help,
the linker call does not include ''-nostdlib'' there do appear to be several library versions, (pic attached) but I can find nowhere in the toolchain where the version is specified or any refernce in the help to doing so. this is a copy of the build log: 'Invoking: MCU GCC Linker' arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -L..\..\..\..\..\..\..\..\Middlewares\ST\STemWin\Lib -specs=nosys.specs -specs=nano.specs -T''..\STM32F429NIHx_FLASH.ld'' -Wl,-Map=output.map -Wl,--gc-sections -lm -o ''STM32F429I_DISCO_MB1elf'' ./Middlewares/STemWin/Config/GUIConf.o ./Middlewares/STemWin/Config/GUI_X.o ./Middlewares/STemWin/Config/LCDConf_stm32f429i_disco_MB1o ./Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal.o ./Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal_cortex.o ./Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal_crc.o ./Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal_dma.o ./Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal_dma2d.o ./Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal_flash.o ./Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal_flash_ex.o ./Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal_gpio.o ./Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal_i2c.o ./Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal_i2c_ex.o ./Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal_i2s.o ./Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal_i2s_ex.o ./Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal_ltdc.o ./Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal_pwr.o ./Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal_pwr_ex.o ./Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal_rcc.o ./Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal_rcc_ex.o ./Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal_rtc.o ./Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal_rtc_ex.o ./Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal_sdram.o ./Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal_spi.o ./Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal_tim.o ./Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal_tim_ex.o ./Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal_uart.o ./Drivers/STM32F4xx_HAL_Driver/stm32f4xx_ll_fmc.o ./Drivers/CMSIS/system_stm32f4xx.o ./Drivers/BSP/STM324x9I_DISCO/stm32f429i_discovery.o ./Drivers/BSP/STM324x9I_DISCO/stm32f429i_discovery_io.o ./Drivers/BSP/STM324x9I_DISCO/stm32f429i_discovery_sdram.o ./Drivers/BSP/STM324x9I_DISCO/stm32f429i_discovery_ts.o ./Drivers/BSP/Components/ili9o ./Drivers/BSP/Components/stmpe8o ./Application/User/calibration.o ./Application/User/main.o ./Application/User/rtc.o ./Application/User/stm32f4xx_it.o ./Application/SW4STM32/startup_stm32f429xx.o ./Application/Demo/GUIDEMO.o ./Application/Demo/GUIDEMO_AntialiasedText.o ./Application/Demo/GUIDEMO_Automotive.o ./Application/Demo/GUIDEMO_BarGraph.o ./Application/Demo/GUIDEMO_Bitmap.o ./Application/Demo/GUIDEMO_ColorBar.o ./Application/Demo/GUIDEMO_Conf.o ./Application/Demo/GUIDEMO_Cursor.o ./Application/Demo/GUIDEMO_Fading.o ./Application/Demo/GUIDEMO_Graph.o ./Application/Demo/GUIDEMO_IconView.o ./Application/Demo/GUIDEMO_ImageFlow.o ./Application/Demo/GUIDEMO_Intro.o ./Application/Demo/GUIDEMO_Listview.o ./Application/Demo/GUIDEMO_RadialMenu.o ./Application/Demo/GUIDEMO_Resource.o ./Application/Demo/GUIDEMO_Skinning.o ./Application/Demo/GUIDEMO_Speed.o ./Application/Demo/GUIDEMO_Speedometer.o ./Application/Demo/GUIDEMO_Start.o ./Application/Demo/GUIDEMO_TransparentDialog.o ./Application/Demo/GUIDEMO_Treeview.o ./Application/Demo/GUIDEMO_VScreen.o ./Application/Demo/GUIDEMO_WashingMachine.o ./Application/Demo/GUIDEMO_ZoomAndRotate.o ./Application/Demo/syscalls.o -l:STemWin528_CM4_GCC.a c:/ac6/systemworkbench/plugins/fr.ac6.mcu.externaltools.arm-none.win32_1.3.0.201507241045/tools/compiler/bin/../lib/gcc/arm-none-eabi/4.9.3/../../../../arm-none-eabi/lib/armv7e-m/fpu\libm.a
(lib_a-w_sqrt.o): In function `sqrt': w_sqrt.c:(.text.sqrt+0x9e): undefined reference to `__errno' w_sqrt.c:(.text.sqrt+0xa8): undefined reference to `__errno' collect2.exe: error: ld returned 1 exit status make: *** [STM32F429I_DISCO_MB1elf] Error 1 ________________ Attachments : GCC_Libs.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Htav&d=%2Fa%2F0X0000000aS2%2F1fIcSILBHmiQFYsHpFCflhCqnJHzgHFcQqvEDD7a3So&asPdf=false2015-10-23 06:20 AM
Honestly, I don't know.
Just for curiosity, I installed the system workbench (the 64-Bit version failed on a 64-Bit system, only the 32-Bit version works ...), and test-build a simple application for the F3. Using the SPL, I had no linking issues, even when using sqrt(). The final linker stage call looks like : 'Invoking: MCU GCC Linker' arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=softfp -L''E:\Tools\Ac6\workspace\stm32f3discovery_stdperiph_lib\Debug'' -T''E:\Tools\Ac6\workspace\F3_test\LinkerScript.ld'' -Wl,-Map=output.map -Wl,--gc-sections -lm -o ''F3_test.elf'' @''objects.list'' -lstm32f3discovery_stdperiph_lib so the actual errno variable might reside in stm32f3discovery_stdperiph_lib.a. You could of course add a global ''errno'' variable to your project, but that might break something else ... I rather stick to Crossworks, and avoid the Cube firmware at all costs ...2015-10-23 06:44 AM
Well thanks for trying anyway
Intestingly, my own project throws the same error if I include the sqrt function, but not with other maths functions (sin() etc.)but the demo project still throws the error, referencing sqrt, even if I delete all use of sqrt from the project...???I'll keep working at it for now. I was hoping to get away with a 'free' IDE, but may end up having to persuede my boss to splash out on a pukka Keil ARM-SDK :-(Cheers,... Daemy2015-10-23 08:27 AM
I was hoping to get away with a 'free' IDE, ...
Then have a look at Em:Blocks (http://www.emblocks.org/web/), which is free as well, and worked out-of-the-box (at least for me). And, it includes the clib (which contains _errno) by default. Not sure about that ''System Workbench'' - it seems to work with the same reliability as french cars ...
2015-10-23 09:13 AM
__errno is a function that returns a pointer, look to sys/errno.h and sys/reent.h, so not usually a global variable.
I've been building GNU/GCC code with makefiles, and not had this issue, I #include <math.h>, and have the following command lineCompiling file: main.c
arm-none-eabi-gcc -c -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16
-Os -ffunction-sections -fdata-sections -Wall -Wstrict-prototypes -Wextra -std=gnu89 -g -ggdb3 -fverbose-asm -Wa,-ahlms=out/main.lst -DUSE_STDPERIPH_DRIVER -DSTM32F4XX -DUSE_STM32F4_DISCOVERY -DUSE_USB_OTG_FS -DHSE_VALUE=8000000 -D__FPU_PRESENT=1 -MD -MP -MF out/main.d -I. -Iinc main.c -o out/main.o
Also got a chuckle there as my first car was a 2-cylinder Citroen with a gear shift in the dash...
2015-10-23 11:18 AM
__errno is a function that returns a pointer, look to sys/errno.h and sys/reent.h, so not usually a global variable.
Under Linux, it usually is:
http://linux.die.net/man/3/errno
But since it is here (MCU world) basically an emulation of an OS feature, the actual kind of implementation depends on the toolchain or library.Also got a chuckle there as my first car was a 2-cylinder Citroen with a gear shift in the dash...That was probably before the massive invasion of electronics into automobiles ...