2024-11-17 03:39 AM
I have a bit of code as follows:
str r3, [r0, #68]
ldr r3, [r0, #68]
where [r0, #68] is TIM20.BDTR on a STM32G474. I would expect that the LDR would output the same data that was just stored, however it seems that out outputs the previous data. I also tried putting a DMB between the two instructions but the same result still occurred. Inserting 5 DMB instructions seems to cause a long enough delay that the correct data is returned.
This obviously has the potential to be problematic in a few scenarios, but I can't find any documentation from ST on this behaviour, so does anyone know if such documentation exists?
Solved! Go to Solution.
2024-11-17 10:55 AM
Hi @liampwll ,
That is the best workaround :
80128b4: 6c43 ldr r3, [r0, #68] @ 0x44
80128b6: 6c43 ldr r3, [r0, #68] @ 0x44
Just doing a dummy Read back after the first store ! the second LDR will have the right store value.
Cheers,
STOne-32.
2024-11-17 03:49 AM
Never mind, it turns out this is just another case of a key detail being buried in an obscure part of the reference manual:
Because MOE falling edge can be asynchronous, a resynchronization circuit has been inserted between the actual signal (acting on the outputs) and the synchronous control bit (accessed in the TIMx_BDTR register). It results in some delays between the asynchronous and the synchronous signals. In particular, if MOE is set to 1 whereas it was low, a delay must be inserted (dummy instruction) before reading it correctly. This is because the write acts on the asynchronous signal whereas the read reflects the synchronous signal.
- RM0440 Rev 8 28.3.18
However, this still seems to be wrong as a single DMB does not seem to be a long enough delay, so does anyone know what the actual required delay is?
2024-11-17 04:21 AM
Dear @liampwll ,
That register is on APB2 bus, interpretation of cycle is based on it’s own cycles . So if for example the AHBtoAPB2 ratio clock is 4 . One APB2 cycle means 4 AHB or CPU cycles etc.
DMB is acting only at CPU Cortex / AHB cycle to wait till the Internal Cortex-M prefetch is flushed and can not help to wait the APBs mapped registers thru the Bridges . Do you know your AHB/APB2 configuration? And if inline with inserting dummy Reads after the STORE ?
Let us know .
STOne-32
2024-11-17 04:50 AM - edited 2024-11-17 04:52 AM
They're both /1 (HPRE = 0, PPRE = 0). The following works as expected rather than using a DMB, so something about DMB causes an issue even though it should cause at least a single cycle wait as far as I'm aware:
80128ac: 6c43 ldr r3, [r0, #68] @ 0x44
80128ae: f443 4300 orr.w r3, r3, #32768 @ 0x8000
80128b2: 6443 str r3, [r0, #68] @ 0x44
80128b4: 6c43 ldr r3, [r0, #68] @ 0x44
80128b6: 6c43 ldr r3, [r0, #68] @ 0x44
80128b8: 041b lsls r3, r3, #16
2024-11-17 10:55 AM
Hi @liampwll ,
That is the best workaround :
80128b4: 6c43 ldr r3, [r0, #68] @ 0x44
80128b6: 6c43 ldr r3, [r0, #68] @ 0x44
Just doing a dummy Read back after the first store ! the second LDR will have the right store value.
Cheers,
STOne-32.