2024-07-15 07:57 PM - last edited on 2024-07-15 09:54 PM by Peter BENSCH
LDORDY bit does not exist in any registers mentioned in RM0503 rev 2 . I am using ADC1 in STM32U031R6T6 and the code migrated from STM32L010R8T6 is not working .
2024-07-16 12:15 AM
Hello @KSB
Thank you for reporting this issue. Can you give more precision about your request. For the LDORDY bit that is mentioned on the Calibration (ADCAL) part of the RM0503, but it is not mentioned in any register, I've escalated this internally for investigation and correction if necessary.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.