2014-08-01 3:25 AM
Hello, I have a problem with my LCD RX12864H-BIW. I want to use SPI communication but my LCD does not responding. Help me please
#stm32f100rb-spi2014-08-01 7:37 AM
Ok, so have you stuck a Scope or Logic Analyzer on the interface and done any debugging? If so what, and how do the signals correlate with the documentation for the display?
2014-08-04 4:04 AM
The SPI is ok, but the LCD is not responding. I dont know why. The pins is ok, SPI is ok ... I dont know what to do .... here is a photo with the connection
________________ Attachments : 20140804_140011.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I16g&d=%2Fa%2F0X0000000biP%2FVmEV.BBIwq7OXp3a5ai6WSyIJ3JJiBPU_6xiuQLzw7c&asPdf=false20140804_140031.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I16b&d=%2Fa%2F0X0000000biO%2FuS0G9Sg7Uf822zrZb8TaZHYs_vxNRHaleEeoavc_axk&asPdf=false2014-08-04 7:58 AM
I'll see your photos, and raise you some data sheets.
http://teval.ee/media/catalog/product/R/X/RX12864H-BIWRX12864H-BIW.pdf
http://www.tianma-usa.com/web/uploads/controller/20080403002714_ST7567_V0.1.pdf
2015-01-01 9:03 AM
Hello, I have bought a LCD NHD-C12864LZ-FSW-FBW-3V3 with ST7565R.
I use the SPI transmission, with the my STM32VLDISCOVERY board (STM32F100RB) and I do not know why when make the initialization appear few pixels ON. This pixels appear to command ''DISPLAY ON = 0xAF''. Can you help me ? . This is my initialization: void lcd_init(void) { LCD_A0_L(); LCD_N_CS1_L(); LCD_N_RES_H(); delay_ms(500); // Do a hard reset of the LCD display controller LCD_N_RES_L(); delay_ms(500); LCD_N_RES_H(); delay_ms(500); lcd_cmd_out(0xE2); lcd_cmd_out(0XA2); lcd_cmd_out(0XA0); lcd_cmd_out(0XC8); lcd_cmd_out(0XA4); lcd_cmd_out(0XA6); lcd_cmd_out(0X23); lcd_cmd_out(0X81); lcd_cmd_out(0X20); lcd_cmd_out(0X2F); lcd_cmd_out(0X40); lcd_cmd_out(0XAF); // here appear pixels on my LCD delay_ms(500); } When sending the command '' CMD_SET_ALLPTS_ON = 0xA5 '' (All points on ) it is ok. As the attached image. But when sending the command '' CMD_SET_ALLPTS_NORMAL = 0xA4 '' (All points off) it is not ok. As the attached image. Can you help me ? ________________ Attachments : 20141229_004433.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I16M&d=%2Fa%2F0X0000000biN%2F9LGUiIqm70Rnn8FEAUSfgGHWWTZXXZloN9taNpQNYN0&asPdf=false20141229_004704.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I16C&d=%2Fa%2F0X0000000biM%2FYZ1JHIycycFrJC2ACFsYp1e1k7RNGfzSL0SltoDikUU&asPdf=false2015-10-16 12:24 AM
Exactly same error here. Display ON turns all pixel on, when sending all px on or off, no response. logic analyzer though shows correct transmission of the commands