2011-08-08 01:37 AM
hello everybody,
Do you know how to load a binary file into an STM32 Dicovery using Keil (and JTAG), without having the source code? I mean, I do not have a project I can compile, create a binary file and then download it into the board. Do you have any idea how to do it? Thanks in advance.
2011-08-08 05:38 PM
The ST-LINK utilities can download binary files into a VL Discovery board.
Keil is capable of generating Intel Hex, and AXF/ELF object files. Both of which can be converted to binary files.2011-08-08 11:34 PM
Thx a lot clive1, I really appreciate your help.