cancel
Showing results for 
Search instead for 
Did you mean: 

Keil and binary file

edxxgardo
Associate II
Posted on August 08, 2011 at 10:37

hello everybody,

Do you know how to load a binary file into an STM32 Dicovery using Keil (and JTAG), without having the source code? I mean, I do not have a project I can compile, create a binary file and then download it into the board. Do you have any idea how to do it? Thanks in advance.

2 REPLIES 2
Posted on August 09, 2011 at 02:38

The ST-LINK utilities can download binary files into a VL Discovery board.

Keil is capable of generating Intel Hex, and AXF/ELF object files. Both of which can be converted to binary files.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
edxxgardo
Associate II
Posted on August 09, 2011 at 08:34

Thx a lot clive1, I really appreciate your help.