cancel
Showing results for 
Search instead for 
Did you mean: 

Reboot necessary after OTP write?

timothy0508
Associate II

I am using the STM32L432KCU for a project. I intend to use the OTP area for writing persistent device information (serial number, encryption keys, etc).

  1. Is a reboot necessary after writing to the OTP area?
  2. Can the OTP region be written to 32 bits at a time, or does it have be 64 bits?

Thanks

Tim

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
TDK
Guru

No reboot is necessary.

You can only write 64 bits at a time per the reference manual (technically 72 with ECC included).

If you feel a post has answered your question, please click "Accept as Solution".