JLink is not able to detect STM32L476
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-08-26 7:50 AM
We are using STM32L476 Eval board and J-Link Cortex-M JLink_V499a
We flashed the FreeRTOS_LowPower provided in Cube examples through ST-Link , after that J-Link is not able to detect the STM32L476 controller But if we are flashing something which don't have sleep implementation then J-Link is detecting it , as shown below Is it known issue or we are doing something wrong ? Thanks- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-08-26 8:10 AM
Hi horaira,
Please try to connect under Reset.-Syrine-- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-08-26 9:59 AM
Is it known issue or we are doing something wrong ?
Well in some sense, you're removing all power from the chip and expecting it to function normally. Connecting via SWD/JTAG takes some time, one technique is to hold the device in reset while connecting, another is to put the device in System Loader mode to stop your code running. Finally there are DBGMCU settings you can use to keep the connection alive, review the documentation for specifics.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-09-23 9:05 AM
Thanks cliv1,
Problem is that we are not able to flash using j-Link Commander jlink.exe -device ...... as mentioned by you , when we are trying to hold reset and then flash its happening. But we don't want this behavior as in automation build environment no one will be there to hold reset button, I am surprised that why JLink is not using reset pin to reset and halt the device ? Something like with Pre–reset — applies a hardware reset(HW RESET) before connecting to the device. under Reset — holds the hardware reset(HW RESET) signal active while connecting to the device. You may use this option when the user program mistakenly disables the JTAG/SW interface.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-09-23 9:44 AM
Do you have NRST connected on the interface?
You'll have to discuss the J-Link functionality with Segger. You could also consider other programming alternatives, and test fixturing.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-09-24 7:14 AM
Yes, the nRST is connected on Interface
We are using J-Link LITE CortexM Connected Pins are VMCU SWDIO SWCLK SWO nRESET We are stuck, In UM08001 , It seems there is option for STM32 Devices specially to overcome this situation but I don't know how to use it 5.8.2.4 Type 3: Connect under Reset J-Link connects to the target while keeping Reset active (reset is pulled low and remains low while connecting to the target). This is the recommended reset strategy for STM32 devices. This reset strategy has been designed for the case that communication with the core is not possible in normal mode so the VC_CORERESET bit can not be set in order to guarantee that the core is halted immediately after reset.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-09-29 2:58 AM
Dear Clive1,
I posted this in SEGGER forum http://forum.segger.com/index.php?page=Thread&postID=8830#post8830 This is only with STM32L476 or Other Series also have similar behaviour, If yes, How it is being managed ? If we are using ST-Link then this misbehavior is not seen Thanks in advance.