2024-11-21 4:40 AM - last edited on 2024-11-25 7:32 AM by mƎALLEm
Hi,
We are using the STM32U5A9J-DK board and are trying to achieve Read-While-Write (RWW) functionality. The flash chip we are using supports RWW.
Earlier, as per [this post](post link), we learned that to achieve RWW, we need two OSPI instances, namely OSPI1 and OSPI2.
Here are the configurations for both OSPI1 and OSPI2 in STM32CubeIDE:
We tested the setup and observed the following:
Questions:
We would greatly appreciate any insights or guidance on this issue.
Thank you!
2024-12-08 5:11 AM
Hi @KDJEM.1
We are able to do the RWW operation by controlling the CS in software in multiplex mode .
I am able to write to a bank and at the same time able to read the data from another bank.
But there is one thing i need to read the BANKSTAT register to display the error handling and operations going on particular banks.
below is my code for doing that .But i am unable to read the stat register.
I am using READ VOLATILE REGISTER command and address command 0x11 of BANKSTAT to do it can you please tell me whats the issue in below code
2024-12-08 6:04 AM
Probably also want to fix the exit paths so CS goes HIGH, even when unsuccessful
2024-12-12 9:08 PM - edited 2024-12-13 1:23 AM
Hi @Tesla DeLorean ,
Have tried giving exit paths also by giving CS HIGH still unable to read the BANK STAT.Dont know what we are missing.
The Datasheet says First we need to send Command 0x85(READ VOLATILE REG) then the Address of BANK STAT(0x11) followed by dummy cycles (8) then we need to read the DATA,But unable to do it?
Below is the API
uint8_t bankSTATOffset = 4;
uint8_t bankSTATMask = 0x07;
uint8_t bankStatus = 0;
//uint8_t readValue [2] = {0};
OSPI_RegularCmdTypeDef sCommand;
// Step 1: Configure the command to read the volatile register
sCommand.OperationType = HAL_OSPI_OPTYPE_COMMON_CFG;
sCommand.FlashId = HAL_OSPI_FLASH_ID_1;
sCommand.Instruction = READ_VOLATILE_CONFIG_REG;//(0x85) // Read Volatile Register command
sCommand.InstructionMode = HAL_OSPI_INSTRUCTION_1_LINE;
sCommand.InstructionSize = HAL_OSPI_INSTRUCTION_8_BITS;
sCommand.AddressMode = HAL_OSPI_ADDRESS_1_LINE;
sCommand.AddressSize = HAL_OSPI_ADDRESS_8_BITS;
sCommand.Address = READ_BANKSTAT_ADDRESS;//(0x11)
sCommand.DataMode = HAL_OSPI_DATA_1_LINE;
sCommand.NbData = 1;
sCommand.DummyCycles = 8;
sCommand.DQSMode = HAL_OSPI_DQS_DISABLE;
sCommand.SIOOMode = HAL_OSPI_SIOO_INST_EVERY_CMD;
sCommand.AlternateBytesMode = HAL_OSPI_ALTERNATE_BYTES_NONE;
sCommand.AddressDtrMode = HAL_OSPI_ADDRESS_DTR_DISABLE;
sCommand.InstructionDtrMode = HAL_OSPI_INSTRUCTION_DTR_DISABLE;
sCommand.DataDtrMode = HAL_OSPI_DATA_DTR_DISABLE;
HAL_GPIO_WritePin(CS_OSPI_GPIO_Port, CS_OSPI_Pin, GPIO_PIN_RESET);
// Step 2: Send read command
if (HAL_OSPI_Command(&hospi1, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK) {
HAL_GPIO_WritePin(CS_OSPI_GPIO_Port, CS_OSPI_Pin, GPIO_PIN_SET);
Error_Handler(); // Ensure Error_Handler() provides feedback for debugging
}
if (HAL_OSPI_Receive_DMA(&hospi1, &rxBuff) != HAL_OK)
{
HAL_GPIO_WritePin(CS_OSPI_GPIO_Port, CS_OSPI_Pin, GPIO_PIN_SET);
Error_Handler(); // DMA transfer failed
}
HAL_GPIO_WritePin(CS_OSPI_GPIO_Port, CS_OSPI_Pin, GPIO_PIN_SET);
//printf ("The readValue is %x \r\n", rxBuff);
//DebugP_log("RWW write status :0x%X\r\n",rxBuff);
//DebugP_log("RWWContext.BankSize :0x%X\r\n",RWWContext.BANKSize);
#if 1
RWWContext.WriteBANK = rxBuff;
switch (RWWContext.BANKSize)
{
case BANK_4_ARCHITECTURE: bankSTATMask = BANKSTST_REGISTER_MASK_4_BANK_SIZE;
break;
case BANK_8_ARCHITECTURE: bankSTATMask = BANKSTST_REGISTER_MASK_8_BANK_SIZE;
break;
case BANK_16_ARCHITECTURE: bankSTATMask = BANKSTST_REGISTER_MASK_16_BANK_SIZE;
break;
default: break;
}
bankStatus = rxBuff & bankSTATMask;
//DebugP_log("RWW write status :0x%X\r\n",rxBuff);
// printf ("The rxBuff 0x%x\r\n",rxBuff );
// printf("Bank Status: %d\r\n", bankStatus);
// if( ( rxBuff & bankSTATMask) != 0)
// {
// //printf ("The rxBuff 0x%x\r\n",rxBuff );
// return RWWonGoingWriteError;
// }
#endif
return SUCCESS;
One more observation we have is when we do write for Bank 0 in RWW operation whose
sector is from 0-63 we are seeing its effecting even 64th sector the content is being
written to it as well. Similarly, when written to BANK1 and BANK 2, it's getting
effected to BANK2 and BANK3 Respectively. Its only happening to adjacent Banks first sector only.Remaining its not effecting.
How to tackle this?
Regards,
Sanath