Issue using BlueNRG with CubeMX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-05-02 2:19 PM
Hi,
I am using a BlueNRG-MS connected to an STM32L4 MCU over an SPI bus. I was able to make it work using code from the BlueNRG development kit, but I could not make it work if I generated code using CubeMX. After a lot of trial and error, I realized that the CubeMX code was configuring all 4 SPI pins as alternate function (AF5_SPI2), but the BlueNRG example was configuring the slave select pin as an output push pull, which was working. My question is, which is supposed to be correct? As it is, when I enable the SPI2 peripheral in CubeMX, it automatically configures all 4 SPI pins as alternate function, with no other options. I don't know if this is a bug in CubeMX, or if I have some other conflicting configuration that is breaking my setup.
Ricardo
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-05-08 3:02 AM
Hi
Hassan.Ricardo
,Please precise the CubeMX version you are using.
To more understand your request: is your aim touse BlueNRG staring from a project you generate by your self with CubeMX?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-05-08 11:07 AM
Hi Amel,
I’m using STM32CubeMX 4.25.0, with STM32L4 firmware package 1.11.0. Yes, I’m generating my project using CubeMx for a system with a BlueNRG chip.
Regards,
Ricardo
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-05-10 3:52 AM
Hi
Hassan.Ricardo
Could you please give me a link to the dev kit you are using
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-05-10 1:58 PM
This one:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-05-11 4:17 AM
Hi
Hassan.Ricardo
,on this example the SPI CS is also configured as AF
GPIO_InitStruct.Pin = BNRG_SPI_CS_PIN;
GPIO_InitStruct.Mode = BNRG_SPI_CS_MODE; GPIO_InitStruct.Pull = BNRG_SPI_CS_PULL; GPIO_InitStruct.Speed = BNRG_SPI_CS_SPEED; GPIO_InitStruct.Alternate = BNRG_SPI_CS_ALTERNATE; HAL_GPIO_Init(BNRG_SPI_CS_PORT, &GPIO_InitStruct);/* BlueNRG SPI CS define values */
#define SDK_EVAL_V3_SPI_PERIPH_CS_PIN GPIO_PIN_12 /* PB.12 */ #define SDK_EVAL_V3_SPI_PERIPH_CS_MODE GPIO_MODE_OUTPUT_PP #define SDK_EVAL_V3_SPI_PERIPH_CS_PULL GPIO_NOPULL #define SDK_EVAL_V3_SPI_PERIPH_CS_SPEED GPIO_SPEED_HIGH #define SDK_EVAL_V3_SPI_PERIPH_CS_ALTERNATE 0 #define SDK_EVAL_V3_SPI_PERIPH_CS_PORT GPIOB /* GPIOB */ #define SDK_EVAL_V3_SPI_PERIPH_CS_CLK_ENABLE() __GPIOB_CLK_ENABLE()The only difference is that MX doesn't set the state pin when it is an AF like done in this project
HAL_GPIO_WritePin(BNRG_SPI_CS_PORT, BNRG_SPI_CS_PIN, GPIO_PIN_SET);
Could you add this line and test please ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-05-14 12:35 PM
It looks to me that in your example the CS pin mode is configured as output push pull, as you wrote:
&sharpdefine SDK_EVAL_V3_SPI_PERIPH_CS_MODE GPIO_MODE_OUTPUT_PP
The other 3 spi pin modes are configured as alternate function, namely GPIO_MODE_AF_PP. I would have thought that the chip select should also be GPIO_MODE_AF_PP. I'm just trying to confirm that it should be as you wrote above, where the chip select is
GPIO_MODE_OUTPUT_PP.
Ricardo