2017-08-21 2:48 AM
Hello,
In the line 1760 of 'stm32h7xx_hal_adc.c' in pack 'STM32H7xx_DFP 1.0.1':
'''
/* Disable ADC DMA (ADC DMA configuration ADC_CFGR_DMNGT is kept) */
MODIFY_REG(hadc->Instance->CFGR, ADC_CFGR_DMNGT_0 |ADC_CFGR_DMNGT_1, 0);
'''
The comment says 'keep the DMNGT' while the code actually clears it. Besides
it doesn't make much sense to me that calling a 'HAL_ADC_Stop_DMA' could change the initial configuration of ADC.
Is this a bug? Or 'HAL_ADC_Stop_DMA' is not something I should call under normal condition?
2017-08-23 9:02 AM
Hi
aaron_chang
,It seems the comment 'Disable ADC DMA (ADC DMA configuration ADC_CFGR_DMNGT is kept)' creates confusion for you.
In fact here,ADC_CFGR_DMNGT have to be cleared because the call ofADC_ConversionStop doesn't clear them: they are kept as they are.
So this is not a bug.
HAL_ADC_Stop_DMA may be useful in an application where ADC configuration needs to be modified for example to start with a new mode.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.