2021-02-18 06:14 AM
Hi,
i develop 100% of my code in my workshop or office, but sometimes i wish i could do some very light modification to a parameter or baud or something in the field and i dont really fancy carrying my expensive workstation laptop around.
So i wonder if there is an app for android (or ios) similar to stlink utlity, so i could connect st-link debuger via otg usb to tablet and flash new code(modifing can be done easly in any notepad type app) in the field?
Solved! Go to Solution.
2021-02-19 05:53 AM
"what exactly deaf and drop programming is? Google does not find anything useful"
😂
Pretty sure that should be, "drag and drop" ?!
ie, where the ST-Link appears as a USB Mass-Storage Device, so you can just drag your .bin file from wherever you keep it, and drop it onto the ST-Link's MSD.
2021-02-18 06:42 AM
Any STLINK > V1 offers a mass storage device for deaf-and drop programming.Is'nt that what you need?
2021-02-18 08:58 AM
you could try remote desktops, aydesk works well for me
2021-02-19 12:56 AM
thk, will try with aydesk. Tried to make it work with google remote desktop, but didnt have any luck with sharing tablet USB port with pc running the St-link.
2021-02-19 12:57 AM
can you post link to a white paper or some explanation of what exactly deaf and drop programming is? Google does not find anything useful.
2021-02-19 02:03 AM
*anydesk (typo)
2021-02-19 05:53 AM
"what exactly deaf and drop programming is? Google does not find anything useful"
😂
Pretty sure that should be, "drag and drop" ?!
ie, where the ST-Link appears as a USB Mass-Storage Device, so you can just drag your .bin file from wherever you keep it, and drop it onto the ST-Link's MSD.
2021-02-19 05:56 AM
"some very light modification to a parameter or baud or something in the field"
Surely, it would be far better to give your app a configuration interface for such changes - not the kind of thing you want to be rebuilding the code for?
2021-02-19 05:58 AM
Ok, now i feel double stupid, for not getting he meant DRAG and drop and for not thinking of it in first place. Thank for claryfiny it.
2021-02-22 04:47 AM
depends on the project. Most of mine are compiled in few seconds, maybe half a minute tops, so really, rebuilding code is not a problem. And tried this weekend using CubeIDE and anydesk remote, with drag and drop programing via stlink. it all work together as a charm.
But yea, in case of big project with budget for development of interface to set parameters via usb connection and a simple terminal program on tablet side, this is viable solution.