cancel
Showing results for 
Search instead for 
Did you mean: 

Is there a ST-LINK_CLI.exe for ST-Link /V2?

jai2
Associate
Posted on August 09, 2011 at 08:16

Hi All,

I want to use ST-Link/V2 for downloading to flash in KEIL IDE.

At present when you use the flash loader to download. It does not do anything no

error nothing. just does not download

it just says

Load ''D:\\Keil_MDK\\ARM\\INC\\ST\\3.5\\STM32F10x_StdPeriph_Lib_V3.5.0\\Project\\STM32F10x_StdPeriph_Template\\MDK-ARM2\\STM32100E-EVAL\\STM32100E-EVAL.AXF''

Is there a ST-Link_CLI.exe for ST-Link/V2.

In keil I want to do external flash programming.

Thanks and Regards,

Jai

2 REPLIES 2
felipe
Associate II
Posted on March 01, 2013 at 20:02

Same problem for me...

What can I do?

Amel NASRI
ST Employee
Posted on April 02, 2013 at 12:04

Hello Felipe,

''Same problem for me...'', how exactly?

Issue with the FlashLoader? Please note that allowed file formats are .bin, .hex or .s19 and not .axf.

If you are looking for the ST-LINK_CLI.exe, it is available with the ST-Link Utility package downloadable from

http://www.st.com/web/en/catalog/tools/PF258168

.

Best Regards,

ST.MCU

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.