cancel
Showing results for 
Search instead for 
Did you mean: 

Is STM32F429VE (512 KB flash and 100Pins) Micro-controller supports firmware written in HAL APIs from STMicroelectronics ?

gaurav  kumar
Associate II
Posted on May 05, 2017 at 10:56

Hello,

Is STM32F429VE (512 KB flash and 100Pins) Micro-controller supports firmware written in HAL APIs from STMicroelectronics ? 

#stm32-f4 #stm32f429ve
2 REPLIES 2
Nesrine M_O
Lead II
Posted on May 05, 2017 at 12:03

Hi

Kumar.Gaurav.004

,

What do you mean by '

supports firmware written in HAL APIs from STMicroelectronics ? '

Could you please provide more explanation on your case, so that it will be easier to understand the issue?

-Nesrine-

Posted on May 05, 2017 at 13:30

HAL, SPL, register level if you want.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..