2015-07-01 8:05 AM
Hello,
Since I had only bugs with previous versions, I have updated the cubeMX package. It produce the same bug in all following configurations :- cubeMX + IAR- cubeMX + SW4- cubeMX as eclipse plugin + SW4Create a new project, STM32F405 for instance, use ADC, click on ''generate code'' and try to compile.1/- WHY does the *.ioc is copied in a subfolder ? Which one must be used later ?2/- The adc.c/adc.h files are placed in the scr/inc folders (that's the only good news) BUT when compiling gcc reports ''adc.h not found''Other bug :3/-''File/save project as'' (or associated icons) sometime opens the ''settings'' window and sometime opens the ''save as'' windows (randomly).Thank you #worst-forum-software-ever2015-07-01 10:42 AM
Is that like asking if it's bug free, or something?
2015-07-02 7:03 AM
Hello,
1- Do you mean that there are 2 locations for .ioc file?2- Are you facing a compilation issue with IAR?3-''3/-''File/save project as'' (or associated icons) sometime opens the ''settings'' window and sometime opens the ''save as'' windows (randomly)'' if you can clarify this point.Syrine2015-07-02 7:48 AM
Hi,
First of all, stm32cubemx v4.8 is an official version and not a beta one. Second, I generated a new project with IAR and Atollic (because I don't have SW4STM32 installed), and I didn't have neither *.ioc duplicated nor error compilation with gcc. Third I didn't have a problem with saving projects also. RegardsHello,
1- Do you mean that there are 2 locations for .ioc file? 2- Are you facing a compilation issue with IAR? 3-''3/-''File/save project as'' (or associated icons) sometime opens the ''settings'' window and sometime opens the ''save as'' windows (randomly)'' if you can clarify this point. Syrine2015-07-02 8:34 AM
(thanks to notepad++ and CTRL+C/CTRL+V shortcuts. Does the ST forum developers work on a gameboy or why the message box is 85chars * 4 lines ?)
1/double ioc file.1- I took the ioc file from my associate2- Put it into a new, fresh and empty folder3- click ''generate code'' => the code is placed in a subfolder, and a second ioc file was placed in this subfolder. It looks to be a copy of the original ioc file4- regenerating code from the first ioc don't works anymore (cubeMX freeze)5- generating code from the second ioc sometimes works : - the code is sometime placed in the subfolder - the code is sometime placed in the first folder - library (adc.c/h, spi.c/h, sdio.c.h...) are sometime missing - this is absolutely not cool (since 3 days I spent more time debuging cubeMX than my own project) 2/ '' Are you facing a compilation issue with IAR?'' => YES, and SW4STM32 gives the same problems => the errors come from cumeMX.3/ 1- look the icons with 2 floppy drives. According to international standards this icons should be ''save as...''. The infotext is good. Click on this icons and you will see the settings windows.2- Idem with File/save project as3- I *PROMISE* you that yesterday I opened an old project and ''file/save as'' works differently than today. (the ''save as'' command opened the ''save as'' windows)2015-07-02 8:43 AM
Does the ST forum developers work on a gameboy or why the message box is 85chars * 4 lines ?
No it just uses a polished turd from the Microsoft collection, it's like they wanted to join the forum software market 20+ years late, and paid no attention to how stuff could/should work, and found a way to integrate Word(tm) in a fashion that doesn't work on mobile devices, because who uses those in 2015?2015-07-03 9:49 AM
Yesterday night I found a code generation without bug (with all files included).
Today I have to add the sd/fatfs, so, I have to regenerate code with cubeMX. Each time I regenerate code (without any modification of the configuration), the files generated are not the same. The only thing that don't change, is that there is at least one missing file, it can be :- gpio.h- spi.h- spi.c- fatfs.c- bsp_driver_sd.hWhen clicking several time on ''generate'' on the left screen, I see the files (and file number) changing in the inc/ or scr/ folders on the right screen. But when spi.h is present, gpio.c is missing or vice-versa. Obviously the code is never compilable.It is definitely obvious that I am not be the only guy on this planet to have bugs with cubeMX. I hope ST will quiclky solve theses bugs, without introducing new bugs, because I'm not any longer an hobbyist.2015-07-06 12:01 AM
I've similar problem, i solved becouse i've an old .ioc file (for old i mean a backup version before upgrade to 4.8.0). This works perfect.
2015-07-06 1:38 AM
2015-07-17 6:17 AM