cancel
Showing results for 
Search instead for 
Did you mean: 

Is SafeRTOS support in STM32CUBEMX?

Barbie
Associate II

If I want to use the SafeRTOS for critical issue can I use it in the cubeMX as I use today the FreeRTOS?

If it is possible or not at this stage, and if yes what adaptation do I need to do to use it?

Is there any guide for immigrate Safe RTOS to CUBEMX?

Regards

Bar.

1 REPLY 1
AvaTar
Lead

I'd say no.

SafeRTOS is a pre-certified product by Wittenstein, and not freeware.

Licence costs use to be in the 5/6 digit figure range.

> Is there any guide for immigrate Safe RTOS to CUBEMX?

Probably possible, but sounds to me like implanting a Rolls-Royce engine into a golf buggy.