2021-11-18 2:00 AM
Hello!
I have an STM32F411RE nucleoboard.
I tried to use PA2 (TX) and PA3 (RX) as a general output. I enabled the clock access and also setted the mode register to general purpose output mode, but when I connect the LED and set the pin high nothing happens. If I connect it to another pins e.g. PA0 (A0), PA1 (A1), PA8 (D7) it works fine. Could it be because the RX/TX legs can't be used as a general purpose output?
Thanks in advance for the help!
Best regards,
Martin
Solved! Go to Solution.
2021-11-18 8:00 AM
As I said before don't forget to close SB62 and SB63 too, just a bit of tin between the pads will do the job.
2021-11-18 2:18 AM
Hello,
PA2/PA3 can be used as GPIO, but you have to remove SB14 and SB13 to disconnect them from the ST-Link UART interface.
+ check that SB62 and SB63 are set.
2021-11-18 2:22 AM
MCU Tx is output and input on stlink side, so if you can't mingle the solder bridge, that shpuld work.Make sute to program the pin as output push pull.
2021-11-18 7:20 AM
Sorry for this dumb question. Could You show me on the pictures which solder bridge should I remove? I checked the datasheet and I found SB13 and SB14 but I can't see where it joins. I attached 3 pictures about the board.
Thank You! :)
2021-11-18 7:32 AM
I can't show you with your pictures, because it is on the other side of the board.
In UM1724 page 14 Figure 4 "Bottom layout", they are shown.
2021-11-18 7:43 AM
Yes I also found it. Maybe I misunderstood it. When you wrote that I had to remove SB13 and SB14, You meant that I had to remove the transistors from the board? I thought that I had to remove only a jumper.
2021-11-18 7:53 AM
I checked the code it but still not works. The delay is from TIM2_CH1 (PA0). It1s interesting because it worked on PA1 and PA4.
2021-11-18 7:55 AM
Solder Bridges 13 and 14 are 0 Ohm resistors.
They are not jumpers, so you'll have to use soldering iron.
2021-11-18 7:57 AM
Okay, I understand now. :) Thank you!
2021-11-18 8:00 AM
As I said before don't forget to close SB62 and SB63 too, just a bit of tin between the pads will do the job.