cancel
Showing results for 
Search instead for 
Did you mean: 

Is it ok to connect VDDIO2 Pin to VDD?

icecats
Associate

Hi,

I am using STM32L071C8T6 which has a VDDIO2 power pin. I don't see any information on this pin in the STM32L0xx hardware dev reference. My application doesn't require a separate level or source for any GPIO's, so can I connect VDDIO2 directly to VDD?

icecats_0-1716374212586.png

 

Thanks

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello,

According to the datasheet:

SofLit_1-1716374950855.png

So yes you can connect VDDIO2 to VDD.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
SofLit
ST Employee

Hello,

According to the datasheet:

SofLit_1-1716374950855.png

So yes you can connect VDDIO2 to VDD.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.