cancel
Showing results for 
Search instead for 
Did you mean: 

Is it normal for the port reset to be 100ms in the USB Host software? (Min. 10 ms, max. 20ms)

RhSilicon
Lead

Hi,

From RM0090 (Rev 19 - February 2021), page 1393:

"Host enumeration

The application issues an USB reset (single-ended zero) via the USB by keeping the port
reset bit set in the Host port control and status register (PRST bit in OTG_HS_HPRT) for a
minimum of 10 ms and a maximum of 20 ms. The application monitors the time and then
clears the port reset bit."

But apparently the time in the software is 100ms (FW_F4 1.27.1):

stm32f4xx_ll_usb.c

 

 

/**
  * @brief  USB_OTG_ResetPort : Reset Host Port
  *   USBx  Selected device
  * @retval HAL status
  * @note (1)The application must wait at least 10 ms
  *   before clearing the reset bit.
  */
HAL_StatusTypeDef USB_ResetPort(USB_OTG_GlobalTypeDef *USBx)
{
  uint32_t USBx_BASE = (uint32_t)USBx;

  __IO uint32_t hprt0 = 0U;

  hprt0 = USBx_HPRT0;

  hprt0 &= ~(USB_OTG_HPRT_PENA | USB_OTG_HPRT_PCDET |
             USB_OTG_HPRT_PENCHNG | USB_OTG_HPRT_POCCHNG);

  USBx_HPRT0 = (USB_OTG_HPRT_PRST | hprt0);
  HAL_Delay(100U);                                 /* See Note #1 */
  USBx_HPRT0 = ((~USB_OTG_HPRT_PRST) & hprt0);
  HAL_Delay(10U);

  return HAL_OK;
}

 

 

stm32f4xx_hal_hcd.c:

 

/**
  * @brief  Reset the host port.
  *   hhcd HCD handle
  * @retval HAL status
  */
HAL_StatusTypeDef HAL_HCD_ResetPort(HCD_HandleTypeDef *hhcd)
{
  return (USB_ResetPort(hhcd->Instance));
}

 

usbh_conf.c:

 

/**
  * @brief  Reset the Host port of the low level driver.
  *   phost: Host handle
  * @retval USBH status
  */
USBH_StatusTypeDef USBH_LL_ResetPort(USBH_HandleTypeDef *phost)
{
  HAL_StatusTypeDef hal_status = HAL_OK;
  USBH_StatusTypeDef usb_status = USBH_OK;

  hal_status = HAL_HCD_ResetPort(phost->pData);

  usb_status = USBH_Get_USB_Status(hal_status);

  return usb_status;
}

 

usbh_core.c:

 

/**
  * @brief  USBH_Process
  *         Background process of the USB Core.
  *   phost: Host Handle
  * @retval USBH Status
  */
USBH_StatusTypeDef  USBH_Process(USBH_HandleTypeDef *phost)
{
  __IO USBH_StatusTypeDef status = USBH_FAIL;
  uint8_t idx = 0U;

  /* check for Host pending port disconnect event */
  if (phost->device.is_disconnected == 1U)
  {
    phost->gState = HOST_DEV_DISCONNECTED;
  }

  switch (phost->gState)
  {
    case HOST_IDLE :

      if ((phost->device.is_connected) != 0U)
      {
        USBH_UsrLog("USB Device Connected");

        /* Wait for 200 ms after connection */
        phost->gState = HOST_DEV_WAIT_FOR_ATTACHMENT;
        USBH_Delay(200U);
        (void)USBH_LL_ResetPort(phost);

 

stm32f4xx_hal.c:

 

/**
  * @brief This function provides minimum delay (in milliseconds) based 
  *        on variable incremented.
  * @note In the default implementation , SysTick timer is the source of time base.
  *       It is used to generate interrupts at regular time intervals where uwTick
  *       is incremented.
  * @note This function is declared as __weak to be overwritten in case of other
  *       implementations in user file.
  *  Delay specifies the delay time length, in milliseconds.
  * @retval None
  */
__weak void HAL_Delay(uint32_t Delay)
{
  uint32_t tickstart = HAL_GetTick();
  uint32_t wait = Delay;

  /* Add a freq to guarantee minimum wait */
  if (wait < HAL_MAX_DELAY)
  {
    wait += (uint32_t)(uwTickFreq);
  }

  while((HAL_GetTick() - tickstart) < wait)
  {
  }
}

 

 

STM32H7 (FW_H7 1.11.0)

stm32h7xx_ll_usb.c

 

/**
  * @brief  USB_OTG_ResetPort : Reset Host Port
  *   USBx  Selected device
  * @retval HAL status
  * @note (1)The application must wait at least 10 ms
  *   before clearing the reset bit.
  */
HAL_StatusTypeDef USB_ResetPort(USB_OTG_GlobalTypeDef *USBx)
{
  uint32_t USBx_BASE = (uint32_t)USBx;

  __IO uint32_t hprt0 = 0U;

  hprt0 = USBx_HPRT0;

  hprt0 &= ~(USB_OTG_HPRT_PENA | USB_OTG_HPRT_PCDET |
             USB_OTG_HPRT_PENCHNG | USB_OTG_HPRT_POCCHNG);

  USBx_HPRT0 = (USB_OTG_HPRT_PRST | hprt0);
  HAL_Delay(100U);                                 /* See Note #1 */
  USBx_HPRT0 = ((~USB_OTG_HPRT_PRST) & hprt0);
  HAL_Delay(10U);

  return HAL_OK;
}

 

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
waclawek.jan
Super User

> Is it normal for the port reset to be 100ms in the USB Host software?

Yes. The USB specification states, that

> The reset signaling must be driven for a minimum of 10ms (TDRST).

(USB2.0 7.1.7.5). There is no maximum specified.

JW

View solution in original post

1 REPLY 1
waclawek.jan
Super User

> Is it normal for the port reset to be 100ms in the USB Host software?

Yes. The USB specification states, that

> The reset signaling must be driven for a minimum of 10ms (TDRST).

(USB2.0 7.1.7.5). There is no maximum specified.

JW