cancel
Showing results for 
Search instead for 
Did you mean: 

Is it just me, or is the STM32CubeH7 missing the low-layer API?

Nathan Wiebe
Associate
Posted on December 02, 2017 at 22:01

Is it just me, or is the STM32CubeH7 missing the low-layer API?  I can't seem to select LL instead of HAL on the individual drivers in STM32CubeMX under settings like I can on STM32F7 cube projects.  In the descriptions of the STM32CubeXX download links, they all separately specify HAL and LL libraries as included, but on the H7 they say 'low level HALs' are included (which is an oxymoron if you ask me).  I am looking for a per-peripheral way to avoid using the complex, obfuscated version of the HALs (as you can with F7 parts now by choosing LL)...

3 REPLIES 3
john doe
Lead
Posted on December 03, 2017 at 00:07

there isnt even an LL template in the repository.  they want so bad for you to use the hal, just not bad enough to fix it.  do the texas instruments users have this much trouble with the factory software?

Amel NASRI
ST Employee
Posted on July 11, 2018 at 17:34

LL drivers will be embedded in the version 1.4.0 of STM32CubeH7 package (expected to be available on 18Q4).

https://community.st.com/0D50X00009XkbYxSAJ

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Posted on July 11, 2018 at 17:58

https://community.st.com/0D50X00009XkbYxSAJ

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..