2023-04-18 5:29 AM - edited 2023-11-20 7:48 AM
for example IC2 needs pull up resistor on the board but there is internal pull up options for pins.
I wonder if this is the same. So by setting internal pull up you can skip the pull up resistors on the board. I know that NRST pin has internal pull up resistor.
2023-04-18 7:19 AM
No. internal pull-up has a much higher resistance(~40 kOhm? check data sheet) than a typical I2C pull-up (4,7 kOhm, depending on your setup).
hth
KnarfB
2023-04-24 6:43 AM
I followed example from CubeMX to connect 2 Nucleo boards F446, using I2C and they use internal pull up and it does work. I wonder if I can use for example internal pull up for example for SDMMC.
2023-04-24 7:12 AM
What was the clock speed used in this example?
Keep in mind that this 40 kΩ weak pull-up in combination with line and input capacitances is forming a low-pass filter.
So it depends how long and wide your PCB traces are (rule of thumb is 1 pF/cm length for 0.2mm trace width and 0.2mm height above plane - prepreg thickness) and how many slave devices you have on the bus (I/O pad capacitance - around 5 pF per pad).
For example a 10 cm PCB trace (10 pF) + input capacitance (5 pF) = 15 pF
which gives a rise-time of 1.3 us so not good at all for anything above around 500 kHz.
2023-05-15 9:44 AM
The F446 is an MCU, retagged into the proper forum.
MPU = STM32MP1 LINUX, et al