cancel
Showing results for 
Search instead for 
Did you mean: 

Is FT5426 similar to Ft5336

Mselv
Associate II

HI,

I am using a custom board where i need to devlop a touch driver. I am using FT5426.

I have the complete code of fT5336 as it was used in STM32f746-disco board.

can i just by changing the register AND CONFIGURING the i2c pins accordingly.make the touch driver fror ft5426

Has anyone doen that?

To which driver is ft5426 simlar to can anyone help.

I am trying to integarete Embedded wizard to my project

1 REPLY 1
N Sornakumar
Associate III

@Mselv​  are you complete this project ? because i am also using FT5426 in my custom board