cancel
Showing results for 
Search instead for 
Did you mean: 

interrupt latency with 2 two Identical board

Wleon.1
Associate II

Hi, I am using two Identical board, both board installed with a STM32F733ZE, and both have the same program loaded.

The program is very simple where if an interrupt from PG0, will reset the PWM counter of TIM8. provided with the same interrupt source, I am seeing a const 5us delay on the counter reset, given everything are the same I don't understand why am I still getting a 5us delay ?

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4

Does TIM8 have a prescaler?​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

yes but I have set it to 0

TDK
Super User

It's possible the systick interrupt is delaying the interrupt you want from firing. But far more likely is something is different between the two boards, especially if the delay is constant. 5us is quite a long time in terms of cpu cycles.

Cache will also affect execution speed to some degree, though it should be consistent if the two chips are truly running the same code.

If you feel a post has answered your question, please click "Accept as Solution".

Even with crystals the clocks are not identical.

5 us seems like a lot, and not something I can determine specifically.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..