cancel
Showing results for 
Search instead for 
Did you mean: 

Interrupt handler

fixed-term
Associate
Posted on January 01, 2014 at 06:29

Hello all,

                     I am using a small demo kit where i have one push button so whenever it is pressed so an interrupt will be triggered. can you help me(code) to create and interrupu( falling edge, port A bit 0)
1 REPLY 1
Posted on January 01, 2014 at 11:21

Have you looked at any of the examples included with the Discovery kits and/or Standard Peripheral Library?

You will also need to be aware of

http://www.lmgtfy.com?q=Contact%20Bounce

...