cancel
Showing results for 
Search instead for 
Did you mean: 

Internal trigger connection problem with TIM3 on STM32F373CBT6

Stratos hatz
Associate
Posted on December 02, 2017 at 12:43

Hello,I'm using STM32F373CBT6 in my project and I've  noticed that TIM3 is triggered by TIM19 when ITR=0 and not TIM2 as stated in table 45, page 341 of RM0313 Reference manual. I checked the errata notes and didn't find anything relevant.Anyone had this issue before/can verify?Thanks,Stratos

1 ACCEPTED SOLUTION

Accepted Solutions
Posted on December 02, 2017 at 14:28

That table is a bad joke - there are no TIM21 and TIM22 in 'F373 either.

0690X000006093NQAQ.png

This was in rev.1 of the same RM. Spot the differences.

0690X00000608ttQAA.png

It's a shame that users replace ST's document quality control.

JW

View solution in original post

3 REPLIES 3
Posted on December 02, 2017 at 14:28

That table is a bad joke - there are no TIM21 and TIM22 in 'F373 either.

0690X000006093NQAQ.png

This was in rev.1 of the same RM. Spot the differences.

0690X00000608ttQAA.png

It's a shame that users replace ST's document quality control.

JW

Amel NASRI
ST Employee
Posted on March 07, 2018 at 16:44

Hi

stratos_hatz

‌ &

Waclawek.Jan

‌,

First sorry for loosing this discussion in all the ones we have and managing it so late.

I have just reviewed it again and agree with you that the current content of the table 'TIMx internal trigger connection' in RM0

It is reported and should be fixed in next revision of RM0

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Amel NASRI
ST Employee
Posted on May 14, 2018 at 17:33

Hello,

A new revision of 

http://www.st.com/content/ccc/resource/technical/document/reference_manual/fa/06/c7/15/3b/2a/4c/f1/DM00041563.pdf/files/DM00041563.pdf/jcr:content/translations/en.DM00041563.pdf

 fixing this error was delivered on March 2018.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.