2013-05-16 7:10 AM
Hi all
I've some troubles with the internal temperatur sensor from my stm32f051: If I read the adc_channel16 I get ~1920 as value. Then I calculate the result in this way �C = ((V25 - VSENSE) / Avg_Slope) + 25 = ((1.43V - 1.54V) / 4.3mV/�C) + 25 = -0.58�C But this should be ~22�C. Then I thought, that I could use the factory callibration data. But HOW? If I read the stored value like this ''(*((uint32_t*)0x1FFFF7B8))'' I get 100206271 as ''TS ADC raw data acquired at temperature of 30 �C, V
DDA
= 3.3 V
''. So can anyone help me? Or should I use an external SPI temperature sensor for only measuring with an accuracy of ~1�C? Thank you very mutch and best regards #adc-bandgap #stm32f205-temperature2013-05-30 12:17 AM
Hi!
Regarding these TS_CAL1 and 2 values, are they applicable for the STM32F103 device? Cannot find any references in the manuals or guides. I get the feeling that these values are not available with this device. But maybe there is another solution to get more accurate values of the temperature. Regards Peter