cancel
Showing results for 
Search instead for 
Did you mean: 

Inquiry About STM32 Development Boards with Replaceable MCU (Socket-Based)

dkhilals
Associate

Hello ST support,

As a customer working on a project using STM32, I am looking for STM32 development or evaluation boards that feature a socket-based MCU instead of a soldered one. This allows for easy replacement of the microcontroller during the use of some sensitive operations.

I searched the ST website and other sources but couldn’t find such boards officially offered. Are there any ST development kits or third-party solutions that support this feature? If so, could you please provide details on availability and where they can be purchased?

Thanks in advance for your help!

5 REPLIES 5
STTwo-32
ST Employee

Ahla @dkhilals,

There is not such a public ST solution. You may want to contact our local sales and marketing team for more information. 
Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Pavel A.
Evangelist III

We've considered this for several projects but rejected because of size and cost of the socket compared with the MCU chip. Bottom line, we lean towards "SoM" approach: a small board that contains the MCU with several tightly coupled components (external RAM, oscillator, buffers etc). This board connects to a larger board with one or more edge connectors for mezzanine boards. But due to unique nature of embedded projects it is hard to find a ready SOM for STM32 like these, and producing custom SoMs is costly. Rich folks can afford it.

 

You can presumably mount ZIF sockets for QFP and BGA type designs, but these can be very expensive

Seen EVAL and NUCLEO boards with sockets. Some had keep-out zones, and holes, to mount screw-down type adapter. ST might be able to give you a part# for what they used, and you can float off the current parts. The part# might be in one of the BOM

Might be cheaper/easier to use the NUCLEO's ARDUINO/MORPHO connector and mount your circuitry in a mezzanine fashion.

Other very low cost break-out boards, or SoM might suit depending on your base needs.

Aries and others have sockets, you could use cheaper dual in-line sockets, for standard form-factors where you say breakout a 64-pin IC to a 68-pin DIP

See SMT to DIP

http://www.proto-advantage.com/store/index.php?cPath=2200_2207

https://www.icbreakout.com/collections/breakout-boards-qfp-quad-flat-package

https://www.arieselec.com/product/18108-test-socket-breakout-board/

https://www.adafruit.com/product/1241

https://www.ebay.com/itm/253987571618?_skw=48-pin+socket+adapter&epid=1139142999

https://www.ebay.com/itm/172033572048

https://www.ebay.com/itm/152789573388

 

 

 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Actually, there is at least one ST board with MCU socket:

https://www.st.com/en/evaluation-tools/stm32g0316-disco.html

:)

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice

Hello @gbm 

For this specific case, the main MCU is not mounted on the socket but it is mounted on the  DIL8 Breakable part: 

STTwo32_0-1740297520732.png

Also, CN3 it is used to program external MCUs :

STTwo32_1-1740297632737.png

So, the main MCU is not mounted on a socket.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.