2025-01-22 05:40 AM
Dear community,
my Nucleo H723ZG captures analog signals via channels (see attachment) :
The second one reads a 4-20mA pressure signal from a sensor with the help of an external shunt resistor. After a system reset/reboot, the voltage there is now frozen at 0.021mA which is weird and I start suspecting that this specific analog input port has some issue...Could it be, that the input impedance of analog input ports is configurable and might go to a different state after a reset or software reboot?
Thanks in advance
Kind regards
2025-01-22 06:38 AM
Q: .Could it be, that the input impedance of analog input ports is configurable and might go to a different state after a reset or software reboot?
A: No. Analog input or ADC could be damaged, since your circuits very primitive and doesn't protect uCPU against overvoltage.
You may try to test input to adc using potentiometer.