2019-08-09 3:30 AM
Hi
Pre-purchased microcontrollers (stm32h743i) can increase this frequency up to 480 MHz?
2019-08-09 3:50 AM
Liking ones own posts deprioritizes them.
What step/version of the part?
Can't you just configure the PLL and flash wait states?
2019-08-09 4:11 AM
Hello,
depending on the Revision of the Chip the Maximum frequency might be only 400MHZ, as you can read in the Errata (ES0392) of the Chip under 2.2.20
2019-08-09 4:24 AM
Most of them run well over 500 MHz in my experience.
2019-09-05 7:23 AM
Hi!
If you have MCU with revision Y it is mean that maximum frequency is 400 MHz. I achived 420MHz, but it isn't stable.
So be carefull and do checking the revision register at any time you want to configure CPU clock.
ERRATA:
2019-09-05 8:22 AM
The Y parts topping at +5% seems inordinately low