cancel
Showing results for 
Search instead for 
Did you mean: 

Increase frequency to 480

mkari
Associate III

Hi

​Pre-purchased microcontrollers (stm32h743i) can increase this frequency up to 480 MHz?

5 REPLIES 5

Liking ones own posts deprioritizes​ them.

What step/version of the part?

Can't you just configure the PLL and flash wait states?​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
ffabi
Associate II

Hello,

depending on the Revision of the Chip the Maximum frequency might be only 400MHZ, as you can read in the Errata (ES0392) of the Chip under 2.2.20

Most of them run well over 500 MHz in my experience.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Roma Jam
Associate II

Hi!

If you have MCU with revision Y it is mean that maximum frequency is 400 MHz. I achived 420MHz, but it isn't stable.

So be carefull and do checking the revision register at any time you want to configure CPU clock.

ERRATA:

0690X00000AQoppQAD.png

The Y parts topping at +5% seems inordinately low

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..