cancel
Showing results for 
Search instead for 
Did you mean: 

Incorrect low power current consumption CMWX1ZZABZ

Marcel Blindu
Associate II
Posted on June 21, 2018 at 16:03

Hello,

I design a LoRa aplication with CMWX1ZZABZ module. The schematic which I use is the following:

0690X0000060LMZQA2.png

And the current consumption es 1.2mA. Anybody know which are the errors in the schematic to get 1.65uA of the datasheet of the module.

2 REPLIES 2
Posted on June 21, 2018 at 20:45

Is this question related to STM32?

JW

Marcel Blindu
Associate II
Posted on June 22, 2018 at 10:33

Our application consists of a micro stm32f103 that communicates

with lora module and we assumed that the module automatically

enters into low power but the consumption of the module remains at 1.2mA