cancel
Showing results for 
Search instead for 
Did you mean: 

In the RM0090 TIM2-TIM5 describes master / slave. Is TRGO1 always only from TIM_CHANNEL_1? I'm not able to get the simple example in Figure 174 for timer acting as a prescaler to work.

BFox.1
Associate II
 
10 REPLIES 10

Don't hijack others threads. Start your own, stating the STM32 and hardware you are using, and the problem you came across. You can link to this thread if you think it's relevant.

JW