Skip to main content
gatadivijay
Associate II
October 6, 2022
Question

In STM32F072CBT6, We want to use both CAN (PB8,PB9 and PA11,P12)channels at the same time

  • October 6, 2022
  • 3 replies
  • 842 views

Currently any one of the CAN channel is Working at a time.

Out customer requirement is, they need both CAN channel's need to work at the same time.

Please can you explain me and If you have sample code, please attach here.

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
October 6, 2022

The device only has one CAN controller, you're simply switching the pin mapping to use different pairs

You'll need a part with 2x CAN controllers if you need two

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
gatadivijay
Associate II
October 6, 2022

Ok Can you send me the part number of 2x CAN controllers with same pin compatibility. So we directly replace the part and check.

waclawek.jan
Super User
October 6, 2022

There's no 2xCAN STM32 model in QFP-48.

JW