cancel
Showing results for 
Search instead for 
Did you mean: 

Im Trying to access STM32F401CCU6 in a board i have developed, Using STM32 Cube Programmer with no success.

ETsin.1
Associate II
 
5 REPLIES 5
gbm
Lead III

That's a pity, we feel sorry for you.

Hint: maybe someone could help you if you provided some basic information about you problem / schematic, debug connections etc.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice

Design sounds broken​

Work through the design, fix the errors.​

Check all the power related pins, that it is correctly orientated​.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
ETsin.1
Associate II

It seems i have no problem erasing and programing the uC in old versions of STM programmer. Only the new STM CUBE is not reading the uC.

Here are some schematics:

0693W00000WIH94QAH.png

ETsin.1
Associate II

Programming Connector used:

0693W00000WIHBjQAP.png

Check firmware and cables

Check connectivity modes, and speeds.

Is NRST connected to the debug pod? Needed for "Connect Under Reset" to work as expected.

ST-LINK/V2 or V3, authentic, or clone?

Avoid using USB Hubs or Docking Stations.

With Micro USB cables make sure to use data or USB 2.0 rated cables, and not charging cables.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..