cancel
Showing results for 
Search instead for 
Did you mean: 

Ideas for improvement STM32CubeMX

asrock70
Associate II
Posted on November 20, 2015 at 11:22

1. Timer Configuration

Add the

timer

configuration

calculator

which of

the requested Interupt Time or Frequency calculate Counter Period (ARR) and

conversely

the

input values

shows the parameters

counter.

Excellent

would be

a graphical

display of output

PWM

etc.

2. Timer Configuration

Now

we see Clock Source: Internal clock

Why

not see

currently set

value of Internal Clock?

3.

Graphical

highlighting

functional groups

of pins

For example, When scroll over

UART

in

list

P

inout t

hey might

highlight

pins

occupied

this Peripheral .

If the

periphery of

the conflict

highlight

graphically

what

pin.

This is important

especially

if you

are using

STM32Cube

simultaneously

with the 

hardware (PCB) design.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Nesrine M_O
Lead II
Posted on November 20, 2015 at 15:40

Hi Charles,

Thanks for the suggestion! I will forward this to our team.

-Syrine –

Nickname6528_O
Associate
Posted on November 27, 2015 at 13:42

Hi Charles

Could you be more precise on your request ''1. timer configuration'' : 

- What do you want to use the timer for ?

- What will be the ''inputs'' and the ''outputs'' of what you call ''timer configuration calculator'' : I didn't catch, for example, if you imagine the ''PWM output waveform'' as an Input or an Output.

Concerning ''2. Timer Configuration'' :

- Where do you except to see the ''Internal clock'' value ? Directly in the ''Pinout view'', when selecting ''Clock Source'' (as Internal Clock or  ETR2 or ETR2...)

regards,