2021-09-14 3:44 AM
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/utils.h(160): error: #65: expected a ";"
int32_t lo = (int32_t) ((in << 32) >> 32);
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/utils.h(162): error: #20: identifier "n1" is undefined
n1 = __CLZ(hi) - 32;
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/utils.h(162): error: #20: identifier "hi" is undefined
n1 = __CLZ(hi) - 32;
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/utils.h(168): error: #20: identifier "lo" is undefined
n1 = __CLZ(lo);
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/utils.h(204): error: #20: identifier "lo" is undefined
*normalized = (((uint32_t) lo) >> n1) | (hi << (32 - n1));
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/utils.h(212): warning: #174-D: expression has no effect
int32_t normalized;
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/utils.h(212): error: #65: expected a ";"
int32_t normalized;
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/utils.h(213): warning: #174-D: expression has no effect
int32_t norm;
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/utils.h(213): error: #65: expected a ";"
int32_t norm;
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/utils.h(220): error: #20: identifier "normalized" is undefined
arm_norm_64_to_32u(absNum, &normalized, &norm);
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/utils.h(220): error: #20: identifier "norm" is undefined
arm_norm_64_to_32u(absNum, &normalized, &norm);
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/matrix_functions.h(548): error: #757: function "int32_t" is not a type name
int32_t shift,
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/matrix_functions.h(563): error: #757: function "int32_t" is not a type name
int32_t shift,
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/controller_functions.h(209): error: #757: function "int32_t" is not a type name
int32_t resetStateFlag);
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/controller_functions.h(227): error: #757: function "int32_t" is not a type name
int32_t resetStateFlag);
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/controller_functions.h(246): error: #757: function "int32_t" is not a type name
int32_t resetStateFlag);
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/distance_functions.h(179): error: #757: function "int32_t" is not a type name
float32_t arm_minkowski_distance_f32(const float32_t *pA,const float32_t *pB, int32_t order, uint32_t blockSize);
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/svm_functions.h(65): error: #757: function "int32_t" is not a type name
__STATIC_INLINE float32_t arm_exponent_f32(float32_t x, int32_t nb)
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/svm_functions.h(91): error: #757: function "int32_t" is not a type name
const int32_t *classes; /**< The two SVM classes */
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/svm_functions.h(105): error: #757: function "int32_t" is not a type name
const int32_t *classes; /**< The two SVM classes */
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/svm_functions.h(106): error: #757: function "int32_t" is not a type name
I have included the path but still iam getting this error
Solved! Go to Solution.
2021-09-15 5:28 AM
Hello @Vk.2 ,
To integrate DSP libraries in your project, please follow this FAQ: Configuring DSP libraries on STM32CubeIDE.
Check also the defines and the include libraries.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Imen
2021-09-15 5:28 AM
Hello @Vk.2 ,
To integrate DSP libraries in your project, please follow this FAQ: Configuring DSP libraries on STM32CubeIDE.
Check also the defines and the include libraries.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Imen