cancel
Showing results for 
Search instead for 
Did you mean: 

I3C Dynamic Address

Azad
Associate II

I'm using the I3C_Controller_ENTDAA_IT example to assign dynamic addresses to two BMA530 sensors, but I'm getting errors when running the code. Are there any modifications or additional steps I should consider to resolve this issue? I haven't made any modifications or additions yet.

Azad_0-1721655184264.png

 

1 ACCEPTED SOLUTION

Accepted Solutions

Sorry, my mistake. I needed to load both the controller_entdaa_it and target_entdaa_it codes for the ENTDAA command to work. I had only loaded controller_entdaa_it. The problem is solved now.

View solution in original post

2 REPLIES 2
Douglas MILLER
ST Employee

This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly

Sorry, my mistake. I needed to load both the controller_entdaa_it and target_entdaa_it codes for the ENTDAA command to work. I had only loaded controller_entdaa_it. The problem is solved now.