I2C: where is data from HAL_I2C_Master_Receive_IT()?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-01-08 02:50 PM
Posted on January 08, 2016 at 23:50
Hi,
I'm attempting to read an I2C device withHAL_I2C_Master_Receive_IT(). A logic analyzer shows the data coming across the I2C bus, but where does it go? This is a st32f405, IAR, and CubeMx generated code. Given the logic analyzer results, it seems the I2C bus and CubeMx code is fundamentally working.uint8_t value8;<
br
><
br
>value8 = 0x79;<
br
>halResult = HAL_I2C_Master_Receive_IT(&hi2c1, (uint16_t)FUEL_GAUGE_I2C_ADDRESS, &value8, (uint16_t)1);<
br
>
As I read the HAL documentation, the value read from I2C should be placed at value8. It's not. What am I missing?
A more complete code block is below. The initial write is to configure the I2C slave for the following read. Everything appears correct on the logic analyzer.
uint16_t tmpValue;<
br
> uint8_t value8;<
br
> HAL_StatusTypeDef halResult;<
br
> <
br
> aTxBuffer[0] = 0x06; // cmd<
br
> aTxBuffer[1] = 0x07; // cmd<
br
> <
br
> halResult = HAL_I2C_Master_Transmit_IT(&hi2c1, (uint16_t)FUEL_GAUGE_I2C_ADDRESS, (uint8_t*)&aTxBuffer[0], (uint16_t)2);<
br
> if (halResult != HAL_OK)<
br
> {<
br
> return false;<
br
> }<
br
> <
br
> // Wait for the end of the transfer<
br
> //<
br
> while (HAL_I2C_GetState(&hi2c1) != HAL_I2C_STATE_READY)<
br
> {<
br
> }<
br
> <
br
> HAL_Delay(70);<
br
> <
br
> // Read result<
br
> //<
br
> value8 = 0x79;<
br
> <
br
> halResult = HAL_I2C_Master_Receive_IT(&hi2c1, (uint16_t)FUEL_GAUGE_I2C_ADDRESS, &value8, (uint16_t)1);<
br
> if (halResult != HAL_OK)<
br
> {<
br
> return false;<
br
> }<
br
><
br
> tmpValue = (uint16_t)value8;<
br
> *value = tmpValue;<
br
> <
br
> return true;<
br
>
The result of this block is value8 remains unchanged by the call to HAL_I2C_Master_Receive_IT.
I've tried various lengths for the I2C read and the result is consistent. Thre received data doesn't end up where the HAL documentation seems to say it should.
Steve
#stm32f405-hal-i2c
Labels:
- Labels:
-
STM32F4 Series
3 REPLIES 3
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-01-08 02:55 PM
Posted on January 08, 2016 at 23:55
Seems I didn't do too well with pasting the code blocks.
The first simple code block is:uint8_t value8;value8 = 0x79;halResult = HAL_I2C_Master_Receive_IT(&hi2c1, (uint16_t)FUEL_GAUGE_I2C_ADDRESS, &value8, (uint16_t)1);The larger code block is: uint16_t tmpValue; uint8_t value8; HAL_StatusTypeDef halResult; aTxBuffer[0] = 0x06; // cmd aTxBuffer[1] = 0x07; // cmd halResult = HAL_I2C_Master_Transmit_IT(&hi2c1, (uint16_t)FUEL_GAUGE_I2C_ADDRESS, (uint8_t*)&aTxBuffer[0], (uint16_t)2); if (halResult != HAL_OK) { return false; } //Wait for the end of the transfer // while (HAL_I2C_GetState(&hi2c1) != HAL_I2C_STATE_READY) { } HAL_Delay(70); // Read result // value8 = 0x79; halResult = HAL_I2C_Master_Receive_IT(&hi2c1, (uint16_t)FUEL_GAUGE_I2C_ADDRESS, &value8, (uint16_t)1); if (halResult != HAL_OK) { return false; } tmpValue = (uint16_t)value8; *value = tmpValue; return true;Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-01-08 05:46 PM
Posted on January 09, 2016 at 02:46
Be careful if the variable you are asking it to write under interrupt is a local/auto variable, in a routine you will leave.
If it's filling under interrupt, I presume the functions are non-blocking, and that the value will not be there until the interrupt actually occurs. You leave immediately, is it even done at that point?
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-01-08 07:59 PM
Posted on January 09, 2016 at 04:59
Of course!
Thank you so much, Clive. I really appreciate it!Steve