Question
Installing ST-LINK/V2 USB drivers.
Posted on January 08, 2016 at 22:57
Hi, I'm a newbie, and I have just started working with STM32 and the GNU tools available, and can anybody explain what is correct from the following quote on how to install
which is on (http://gnuarmeclipse.github.io/openocd/install/
) OpenOcd: ST-LINK/V2One example of compatible drivers are the ST-LINK/V2 USB drivers, from ST, available as part number
http://www.st.com/web/en/catalog/tools/FM147/SC1887/PF260219
. Download thestsw-linkzip archive, extract its content to a separate folder, and run the
dpinst_amdexe (or
dpinst_xexe) with administrative privileges.
I Have two versions of OpenOCD
ST-LINK_USB_V2_1_Driver
and
ST-LINK_USB_V2_Driver
Has anyone done it this way before?
Thanks.
#openocd