2020-09-16 4:47 AM
Hello All.
I am trying to establish an I2C communication between STM32F091VCT6 which is configured as a slave and another controller as a master.
I am trying to send data in blocking mode and facing certain issues. I am able to verify an address acknowledgement from stm and able to send a test 1 value data.
I see an issue while transmitting multiple data in a buffer. Using breakpoints, I can see that the code is stuck checking TXIS flag, which never seems to be set and eventually gets timed out.
Any support will be helpful.
I2C initialization code:
hi2c1.Instance = I2C1;
hi2c1.Init.Timing = 0x00101D2D;
hi2c1.Init.OwnAddress1 = 90;
hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c1.Init.OwnAddress2 = 0;
hi2c1.Init.OwnAddress2Masks = I2C_OA2_NOMASK;
hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_ENABLE;
if (HAL_I2C_Init(&hi2c1) != HAL_OK)
{
Error_Handler();
}
/** Configure Analogue filter
*/
if (HAL_I2CEx_ConfigAnalogFilter(&hi2c1, I2C_ANALOGFILTER_DISABLE) != HAL_OK)
{
Error_Handler();
}
/** Configure Digital filter
*/
if (HAL_I2CEx_ConfigDigitalFilter(&hi2c1, 0) != HAL_OK)
{
Error_Handler();
}
Thanks in advance.
2020-09-16 4:57 AM
SDA and SCL lines- 1st image single data and 2nd image buffered data