2024-01-07 11:32 PM
hii,
i am using stm32 nucleo g0-b1re i am trying to receive data in interrupt mode, but cant figure out what is wrong, i am new to stm32 i2c protocol.
i have used master as nucleo-h743zi2 and transmitting data, but it is not showing anything on minicom.
2024-01-08 01:55 AM - edited 2024-01-08 01:57 AM
Hello @Rohit007,
Try this code :
/* USER CODE BEGIN 2 */
/*##- Put I2C peripheral in reception process ###########################*/
if (HAL_I2C_Slave_Receive_IT(&hi2c1, (uint8_t *)aRxBuffer, RXBUFFERSIZE) != HAL_OK)
{
/* Transfer error in reception process */
Error_Handler();
}
/*##- Wait for the end of the transfer ###################################*/
/* Before starting a new communication transfer, you need to check the current
state of the peripheral; if it�s busy you need to wait for the end of current
transfer before starting a new one.
For simplicity reasons, this example is just waiting till the end of the
transfer, but application may perform other tasks while transfer operation
is ongoing. */
while (HAL_I2C_GetState(&hi2c1) != HAL_I2C_STATE_READY)
{
}
/* USER CODE END 2 */
Best Regards,
Pierre
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-08 02:02 AM
actually it is not receiving a single bit of data, it is not entering into address callback function.
2024-01-08 02:07 AM - edited 2024-01-08 02:09 AM
Are you aware of this article? It explains what is I2C is and how to use it through examples.
I advise you to read it if you are new to stm32 I2C protocol. 🙂
What is your application ? Who is the master ?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-08 03:07 AM
my application is to read variable amount of data sent by the master. my master is nucleo- h743zi2 it is sending data of variable amount, i.e. if i send 5 byte my slave should read only that much data or if 10 bytes, slave should be ready to read that too.
2024-01-08 06:32 AM
Use a logic analyzer to understand what is happening on the line.
2024-01-09 05:03 AM - edited 2024-01-09 05:05 AM
Hello @Rohit007,
Here are some remark about what may happen :
Best Regards,
Pierre
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.