Skip to main content
Scribe
Associate II
January 24, 2019
Question

I2C not responding to read sequence on STM32L0

  • January 24, 2019
  • 2 replies
  • 907 views

Hi guys,

I'm using the latest ST generated I2C hal driver on an STM32L0. On my I2C master, I'm requesting to read from a register, which sends the following sequence:

Start -> Address (W) -> Register 1B -> Stop -> Start -> Address (R) -> Data 4B -> Stop

On the slave end, it's receiving the address, which is triggering the address callback, it's matching, it requests to receive 1 Byte via HAL_I2C_Slave_Seq_Receive_IT(), it receives this, the listen complete callback is then raised which re-enables the listen callback. It then receives and seems to correctly handle the request for the slave to send the 4 data bytes, however what ends up on the bus is 0xFF for each byte. I'm unsure why the data isn't being transmitted.

I do have clock stretching turned off (as master doesn't support it) but have tried this at low speeds such as 10KHz.

My code is implemented as follows:

// Setup
while( HAL_OK != HAL_I2C_EnableListen_IT( &hi2c1 ) );
 
void HAL_I2C_AddrCallback(I2C_HandleTypeDef *hi2c, uint8_t TransferDirection, uint16_t AddrMatchCode)
{
 if(AddrMatchCode == 4)
 {	
		if( TransferDirection == I2C_DIRECTION_TRANSMIT )
		{
			while(HAL_I2C_Slave_Seq_Receive_IT( &hi2c1, buffer, 1, I2C_FIRST_FRAME) != HAL_OK);
			mode = I2C_MODE_SET_REGISTER;
		}
		else
		{			
			if( mode == I2C_MODE_RECEIVE_REGISTER )
			{
				buffer[0] = 0xAA;
				buffer[1] = 0xAA;
				buffer[2] = 0xAA;;
				buffer[3] = 0xAA;
				while(HAL_I2C_Slave_Seq_Receive_IT( &hi2c1, buffer, 4, I2C_LAST_FRAME) != HAL_OK);
				mode = I2C_MODE_NONE;
			}	
		}
	}
}
void HAL_I2C_ListenCpltCallback(I2C_HandleTypeDef *hi2c)
{
	while( HAL_OK != HAL_I2C_EnableListen_IT( &hi2c1 ) );
}
 
void HAL_I2C_SlaveRxCpltCallback( I2C_HandleTypeDef *hi2c )
{
	switch( mode )
	{
		case I2C_MODE_SET_REGISTER:
			currentRegister = buffer[0];
			mode = I2C_MODE_RECEIVE_REGISTER;
			break;
 
		default: break;
	}
}

Any ideas?

Many thanks

This topic has been closed for replies.

2 replies

After Forever
Senior III
January 24, 2019

I don't use HAL to know for sure, but it seems you are using the same HAL_I2C_Slave_Seq_Receive_IT function for both receiving and transmitting. Isn't it wrong?

Scribe
ScribeAuthor
Associate II
January 24, 2019

I thought this too, but I've tried both, same result! Also ST example 'I2C_TwoBoards_RestartAdvComIT' uses Receive like this too, I think because it's part of a receive sequence?