2013-11-05 7:51 AM
Hello everybody,
I have an application for the STM32f051 wich has a i2c device connected I have configured and initialized the i2c, however when I send some data both SDA and SDI lines are staying 'high', I don't see any pulses on any of the lines. I have configured the bus like this:/* Connect PXx to I2C_SCL */
GPIO_PinAFConfig(GPIOB, GPIO_Pin_6, GPIO_AF_1);/* Connect PXx to I2C_SDA */
GPIO_PinAFConfig(GPIOB, GPIO_Pin_7, GPIO_AF_1);/*!< Configure I2C pins: SCL */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_OD; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOB, &GPIO_InitStructure);/*!< Configure I2C pins: SDA */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7; GPIO_Init(GPIOB, &GPIO_InitStructure); I have initialized my clocks like this: RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA | RCC_AHBPeriph_GPIOB | RCC_AHBPeriph_GPIOC | RCC_AHBPeriph_GPIOF , ENABLE); RCC_APB1PeriphClockCmd( RCC_APB1Periph_TIM2 | /* for 1ms timer */ RCC_APB1Periph_TIM3 | RCC_APB1Periph_USART2 | RCC_APB1Periph_I2C1 , ENABLE); /* for event timer */ /* Configure the I2C clock source. The clock is derived from the HSI */ RCC_I2CCLKConfig(RCC_I2C1CLK_HSI); I have initialized the i2c bus like this: /* I2C configuration */ I2C_InitTypeDef I2C_InitStructure; I2C_InitStructure.I2C_Mode = I2C_Mode_I2C; //I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2; I2C_InitStructure.I2C_AnalogFilter = I2C_AnalogFilter_Enable; I2C_InitStructure.I2C_DigitalFilter = 0x00; I2C_InitStructure.I2C_OwnAddress1 = 0x00; I2C_InitStructure.I2C_Ack = I2C_Ack_Enable; I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; I2C_InitStructure.I2C_Timing = 0x1045061D; //I2C_TIMING;/* Apply I2C configuration after enabling it */
I2C_Init(I2C1, &I2C_InitStructure);/* I2C Peripheral Enable */
I2C_Cmd(I2C1, ENABLE); Can anyone say what i'am doing wrong? Thanks in advance, Evert #stm32f051-i2c-init2013-11-05 7:59 AM
PinAFConfig needs PinSource (index) not Pin (mask) values.