2018-08-16 4:26 PM
Hi,
I am working on I2C read EEPROM. The HAL function failed due to the I2C_FLAG_BUSY is always SET.
Is there anything I am missing in init code?
Thx
if (I2C_WaitOnFlagUntilTimeout(hi2c, I2C_FLAG_BUSY, SET, I2C_TIMEOUT_BUSY, tickstart) != HAL_OK)
{
return HAL_TIMEOUT;
}
2018-08-17 4:42 PM
m_i2c->read_from_address(0b10100000, 0xFA, 1, in_data, in_len);
that's incorrect.
read is 0b10100001
2018-08-17 4:48 PM
You are right. I correct it OR to 0x01. Thx
2018-08-17 4:56 PM
works now ?
now we find the next issue :(
its a difficult struggle to bring up code on a new chip.
best not to use blocking code, otherwise you will continually have issues...
2018-08-20 8:53 AM
No, I corrected the READ command after you but still failing.
This is our existing driver for NXP MCP5777m. I just ported to STM32. Still seeing issue and it's on STM32 side for all of checking before sending I2C data out.
I am wondering if the init code not quite right. I am using MXCube code.
Thx
2019-01-16 5:40 PM
Hi,
I'm using HAL_I2c_Mem_Read(), too.
And may I ask if STM32's I2C can generate wave like the following picture. I have tryed Mem_read() and any other function in i2c.c , but the bit following device addres is "0",which means "write" in I2c.
May you help me out, thanks.
2019-01-16 5:52 PM
Yes, that doesn't look like the usual I2C method, which is to have a WRITE with the Register Address, and then a READ which pulls the data.
Probably going to need to bit-bang the frame here.
2019-01-16 6:07 PM
thanks for your reply,
I have bit-bang and success, but I just want to know may stm32's i2c hsrdware generate the ware, by the way the chip is infineon's tle493d-A2B6.
have a nice day.
2023-06-06 4:08 PM
This is often because you don't have pull-ups on the SDA and/or SCL lines (4.7k-10k). You can also enable the internal pull-ups in the MCU itself.
2023-06-06 10:58 PM - edited 2023-11-20 9:40 AM
24AA02E48/25E48/24AA02E64/25E64 Data Sheet (microchip.com)
Notice the Restart bit in the middle? That is true I2C.
It does not match your reference shared document.
Same device, really?