2012-10-31 1:57 PM
I am communicating with a slave device and after the generation of the start condition, I am not seeing SCL and SDA pulsing. Below is the code:
void DS2482_Init(void){ GPIO_InitTypeDef GPIO_InitStructure; I2C_InitTypeDef I2C_InitStructure; /* Enable peripheral clock */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C2, ENABLE); /* Enable GPIOB clock */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE); /* Configure I2C2_SCL and I2C2_SDA */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_OD; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOB, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11; GPIO_Init(GPIOB, &GPIO_InitStructure); /* Enable I2C2 reset state */ //RCC_APB1PeriphResetCmd(RCC_APB1Periph_I2C2, ENABLE); /* Release I2C2 from reset state */ //RCC_APB1PeriphResetCmd(RCC_APB1Periph_I2C2, DISABLE); I2C_DeInit(DS2482_I2C); /* DS2482 peripheral configuration */ I2C_InitStructure.I2C_Mode = I2C_Mode_I2C; I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2; I2C_InitStructure.I2C_OwnAddress1 = DS2482_I2C_ADDRESS; I2C_InitStructure.I2C_Ack = I2C_Ack_Enable; I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; I2C_InitStructure.I2C_ClockSpeed = DS2482_I2C_SPEED; /* enable the I2C peripheral */ I2C_Cmd(DS2482_I2C, ENABLE); I2C_Init(DS2482_I2C, &I2C_InitStructure); }int DS2482_channel_select(int channel){ // select the 1-wire channel on DS2482-800 // Returns: TRUE if channel selected // FALSE if device not detected unsigned char ch, ch_read, check; /* while the bus is busy */ while(I2C_GetFlagStatus(DS2482_I2C, I2C_FLAG_BUSY)); /* send START condition */ I2C_GenerateSTART(DS2482_I2C, ENABLE); /* test on EV5 and clear it */ while(!I2C_CheckEvent(DS2482_I2C, I2C_EVENT_MASTER_MODE_SELECT)); //I2C_AcknowledgeConfig(DS2482_I2C, ENABLE); /* Send DS2482 address for write */ I2C_Send7bitAddress(DS2482_I2C, DS2482_I2C_ADDRESS, I2C_Direction_Transmitter); #i2c-example-stm322012-11-01 3:41 AM
I had the same problem yesterday : found a fix like this :
I2C_Send7bitAddress(DS2482_I2C, DS2482_I2C_ADDRESS, I2C_Direction_Transmitter);
becomes :
I2C_Send7bitAddress(DS2482_I2C, (DS2482_I2C_ADDRESS<<1), I2C_Direction_Transmitter);
It appears you need to shift manually... It's quite a bit strange with a complete library from ST.
Is there any i2c config flag to set a different way ?
2012-11-01 12:41 PM
Thanks for pointing it out! I double checked and yes, the slave address needs to be shifted. It is working now :).
2013-02-25 3:02 AM
Hi Stephane,
This shouldn't be a bug as the address is a user defined parameter. The correct format is specified in reference manuals (The 7 bit device address...is placed in the most significant bits of the byte. The eighth bit can be a zero or one.). Best Regards, ST.MCUTo give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.