cancel
Showing results for 
Search instead for 
Did you mean: 

I would like to design IR thermometer non-contact. Please suggest me as MCU with 48(preferred) or 64 pins, ADC 16 bit, with Timer, SPI, I2C, UART, Program memory 16 to 128kB, Zero-Drift Amplification (optional)

AKUMA.2
Associate II

Microcontroller low cost for home health care design

2 REPLIES 2

Isn't there a parameter search tool on the website or within CubeMX?

Most STM32 have 12-bit ADC.

Where do you see most of the 48 pins consumed here? ​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thank you Clive,

However I am looking for 16BIT ADC with low cost solution.

The LCD will be using some of the pins here and some GPIOs for other functionality.