2019-08-07 05:30 AM
I use the LPTIM to schedule tasks but I'm encountering a proble. even when I start the timer the interrupt is not occurring even though I have enabled the Autoreload Interrupt. I have attached an image of the SFR window. At the moment I have just initialised the timer and blibking a LED in the ISR.