I want to use the complementary PWM feature in counters except for two advanced timers(because I have a large number of pulses).
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-06-05 12:43 PM
I have mastered and timed two timers and can produce both pwm and not pulse. But my problem is that there is no dead time between pulses.
Can you suggest a way for me to have an option like ch1ch1n in other timers that have dead time?
- Labels:
-
TIM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-06-05 2:49 PM
What's the problem with Advanced timers, exactly?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-06-06 7:39 AM
I have used advanced timers and I need to have more pulses with a specific dead time.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-06-06 7:42 AM
I actually need 6 Plus. (3 pulses (not) are other pulses). I have generated 4 pulses with two timers 1 and 8 and I need to generate two more pulses, but I can not produce deade time with advanced timers
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-06-06 10:26 AM
in other words
If I want to have the output (ch1ch1n) that is in timers 1 and 8 and can be produced for dead time pulse in other timers as well.
For further explanation, I have slave and master the two timers together and produce a normal pulse in the master timer and a pulse in the sleeve knot timer. But the problem is dead time.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-06-06 1:07 PM
Then use an STM32 model which has more timers with complementary outputs.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-06-07 11:01 PM
I wrote this code, unfortunately, the accuracy of ARR and CCR is in seconds and does not produce waveforms in microseconds.
Can you suggest a solution to increase the accuracy and resolution of the generated pulses ?????
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_ADC1_Init();
MX_TIM2_Init();
MX_TIM3_Init();
MX_TIM4_Init();
MX_UART4_Init();
MX_TIM7_Init();
/* USER CODE BEGIN 2 */
TIM2->PSC = 10000 - 1;
TIM2->DIER = TIM_DIER_CC1IE | TIM_DIER_UIE;
TIM2->ARR = 16000;
TIM2->CCR1 = 8000;
TIM2->CR1 = TIM_CR1_CEN;
TIM7->PSC = 10000 - 1;
TIM7->DIER = TIM_DIER_UIE;
TIM7->ARR = 1600;
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
HAL_UART_Transmit(&huart4,(uint8_t*) "Salam\r\n", 7, 10);
HAL_Delay(1000);
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
AND
void TIM2_IRQHandler(void)
{
/* USER CODE BEGIN TIM2_IRQn 0 */
if((TIM_SR_CC1IF & TIM2->SR) != 0)
{
MLED_GPIO_Port->BSRR = (MLED_Pin<<16);
GM1_GPIO_Port->BSRR = (GM1_Pin<<16);
// HAL_GPIO_WritePin(MLED_GPIO_Port,MLED_Pin,GPIO_PIN_RESET);
// HAL_GPIO_WritePin(GM1_GPIO_Port,GM1_Pin,GPIO_PIN_RESET);
status = 1;
}
if((TIM_SR_UIF & TIM2->SR) != 0)
{
MLED_GPIO_Port->BSRR = (MLED_Pin);
GM2_GPIO_Port->BSRR = (GM2_Pin<<16);
// HAL_GPIO_WritePin(MLED_GPIO_Port,MLED_Pin,GPIO_PIN_SET);
// HAL_GPIO_WritePin(GM2_GPIO_Port,GM2_Pin,GPIO_PIN_RESET);
status = 2;
}
TIM7->CNT = 0;
TIM7->CR1 = TIM_CR1_CEN;
/* USER CODE END TIM2_IRQn 0 */
// HAL_TIM_IRQHandler(&htim2);
/* USER CODE BEGIN TIM2_IRQn 1 */
TIM2->SR = TIM7->SR & (~(TIM_SR_UIF | TIM_SR_CC1IF));
/* USER CODE END TIM2_IRQn 1 */
}
/**
* @brief This function handles TIM3 global interrupt.
*/
void TIM7_IRQHandler(void)
{
/* USER CODE BEGIN TIM7_IRQn 0 */
if(status == 1)
{
GM2_GPIO_Port->BSRR = (GM2_Pin);
// HAL_GPIO_WritePin(GM2_GPIO_Port,GM2_Pin,GPIO_PIN_SET);
status = 0;
}
else if (status == 2)
{
GM1_GPIO_Port->BSRR = (GM1_Pin);
// HAL_GPIO_WritePin(GM1_GPIO_Port,GM1_Pin,GPIO_PIN_SET);
status = 0;
}
TIM7->CR1 = TIM7->CR1 & (~TIM_CR1_CEN);
/* USER CODE END TIM7_IRQn 0 */
// HAL_TIM_IRQHandler(&htim7);
/* USER CODE BEGIN TIM7_IRQn 1 */
TIM7->SR = TIM7->SR & (~TIM_SR_UIF);
/* USER CODE END TIM7_IRQn 1 */
}
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/