cancel
Showing results for 
Search instead for 
Did you mean: 

I want to use STM32G series for SDIO, so that I can use eMMC card. we can not use other stm32 controller.

NANWA.1
Associate II

Dear Sir,

we are using STM32G series controller in our project but the problem is that we are also using eMMC card with 4GB which work on SDIO connectivity.

could you plese share me which STM32g series will be suitable for it.

Thank you

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

Neither the STM32G0 nor the STM32G4 families support SDMMC operation. However, you could use the card in SPI mode at reduced bandwidth. Both families can do SPI.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

1 REPLY 1
TDK
Super User

Neither the STM32G0 nor the STM32G4 families support SDMMC operation. However, you could use the card in SPI mode at reduced bandwidth. Both families can do SPI.

If you feel a post has answered your question, please click "Accept as Solution".