2018-09-24 10:01 AM
should i buy evaluation board if so whch one is better or any online tutorial available
2018-09-24 10:25 AM
STM32F151RCT8 doesn't sound like an actual part number, why this one specifically?
https://www.st.com/en/evaluation-tools/32l152cdiscovery.html
The NUCLEO or DISCO series boards are a good low cost choice.
The L0 or L4 series parts might be a better choice today.
Joseph Yiu's Essential Cortex-Mx book series is pretty good
Each of the parts has a Data Sheet, Reference Manual and Programming Manual, search for the specific part(s) of interest, and go to the Resources portion of the page.
Get some generalized training on micro-controllers, and STM32 parts. Wealth of YouTube videos if you care to browse.
2018-09-24 03:57 PM
I would suggest that you download the Processor Datasheet first to see if this part has all the functions that you want.
after you select a chip, then a Nucleo board is good, you can view the console output in the PC Terminal window.
or else, as @Community member suggested a discovery board, they come with an LCD display.
alternatively;
If you look at these displays: BuyDisplay.com
https://www.buydisplay.com/default/4-3-tft-lcd-display-module-controller-board-serial-spi-i2c-mcu
this one has a SPI interface to a 4.3"
but it is not trivial to get it all up and running, hence Clive's suggestion of Discovery boards, which come with LCD and Demo samples.
2018-09-24 08:51 PM
not perticularly stm32f151rct i just want to understand any stm32f series device for integrating it in my systems and i am using coIDE for programming but i am not able to get any help related to that or any link related to that